Share |
FAQ

Q. Why is my dehydrator running constantly?

A. Excessive leakage or a faulty compressor can cause a dehydrator to run constantly. A dehydrator will operate continually when it is not capable of supplying the airflow demanded by the pressurization system. Leakage in the transmission line or connections can be large enough to cause excessive operation. Check the polytubing and all transmission line connections for leakage. Use a commercial leak detector or soapy water on joints. Bubbles indicate leaks. A dehydrator compressor that is worn beyond its useful life also can force the unit to run constantly.

Q. What do I do if there is a build-up of water in the filter bowls?

A. The problem is most likely with the compressor where the pressure output has dropped. Alternatively, there may be a blockage in the brass fitting positioned below the bowl. Remove the filter bowl and clean the orifice at the base, check for small air flow if none test the compressor. The compressor may need to be rebuilt.

Q. What type of fittings are required to install my dehydrator?

A. All fittings are included in the installation kit that comes with the Andrew dehydrator you have selected.

Q. The dehydrator has been properly fitted, yet there is a small amount of leakage. Is this normal?

A. Yes. There will always be a small leak of between 1 and 5 percent in your system. On the MT/XT Series of dehydrators, leakage increases to 4-8 percent because of feedback through the membrane.

Q. What spare parts should I keep on hand?

A. The operator's manual for every Andrew dehydrator includes a list of replacement parts for the unit.

Q. Does my compressor require lubrication?

A. No. All Andrew-manufactured dehydrators use oil free compressors with sealed bearings.

Q. On my X Series dehydrator, the alarm contacts do not read "open" or "closed". Why is this?

A. Andrew X Series monitors use solid state relays which do not indicate an "open" or "closed" circuit (as a form "C" dry contact relay would). The X Series unit power does not come on and the power switch does not light up. Check the unit's power cord to make sure that it is pressed completely into the IEC socket on the unit.

Q. When using an X Series line monitor, a low pressure alarm is signaled for ports not in use. How can I correct this?

A. Check the unit to make sure that the dip switch is set for the correct number of ports being used. (Refer to the owner's manual for the specific unit.). Or, cap the unused ports and open the valves at the bottom of the flow meters.

Q. The dehydrator cycles on, then off very rapidly. Does this indicate a problem?

A. This may not be a problem with the dehydrator at all. Rapid on-off cycling usually indicates that the dehydrator is able to pressurize the system volume very quickly. Check to see that the valves are open to the waveguide. Rapid cycling may indicate that the dehydrator is too large for the system.

Q. Is a bigger dehydrator better?

A. Not necessarily. A properly sized dehydrator for your system will work best. First, determine the total waveguide volume. Then, using the Andrew catalog or PSI Select software, select a dehydrator that is matched to that volume having the other features desired.

Q. How often should I change the filters in the water bowls?

A. Filters should be changed every 3,000 hours, or when the compressor is rebuilt. Replacement filters are included in the unit overhaul kit.

Q. Can I use my dehydrator to purge the waveguide?

A. Yes. All Andrew dehydrators can be run to purge the waveguide. This extended run will not damage the dehydrator.

Q. Why does the MT050 compressor run so often?

A. The MT050 has an internal air tank that is used to provide a dry air source for the bleed air used to keep the membrane tube dry. The run cycle is not dependent on system volume or condition.

Q. When do I need to rebuild the compressor in my dehydrator?

A. The compressor should be rebuilt at least every 3,000 hours.

Q. Does the black tubing hold up to ultraviolet?

A. Black tubing contains an ultraviolet inhibitor, which is recommended for use in sunlit areas and in close proximity to high ultraviolet light sources.


 
Blog | Contact Us | Careers | My CommScope | Support | Terms of Service | Follow us on: CommScope on Twitter CommScope on LinkedIn
CommScope
FEEDBACK