Hotel Clarion Suites Cannes
Clarion Suites Cannes Croisette leverages RUCKUS® to upgrade its Wi-Fi system
Best in class Wi-Fi for demanding guests
![Hotel-Clarion-Suites-Cannes-case-study-hero500](/globalassets/digizuite/913060-hotel-clarion-suites-cannes-case-study-hero500.jpg?mediaformatid=-1)
Located a few hundred meters from the famous Promenade de la Croisette and the beaches of Cannes, Clarion Suites Cannes Croisette is a 4-star tourist residence with 116 apartments. The residence also boasts two seminar rooms that are available to hotel guests as well as external organizations for professional gatherings, team meetings and general meetings. The hotel welcomes an average of 38,000 guests a year.
Until 2017, the residence was equipped with access points located outside the rooms in the hotel’s corridors. However, since the building’s structure is made of reinforced concrete, Wi-Fi waves did not spread well in the hotel, limiting the range of access points, and guests had difficulty connecting.
Discover the strategy put in place to enhance the hotel’s connectivity and meet their guests‘ demand.